Other Parts Discussed in Thread: TPS629210
Tool/software:
Hello
We are doing the line transient test now. The output of TPS629210 is unstable while the Vin blow 8.6V, with fully loaded I A (Test condition: Vout =3.3V, I-load = 1A @25℃). According to the datasheet, the input voltage range is 3V to 17V, the output current is up to 1A. Could you help to check what wrong with this test or the Buck?
Channel 1 is the Vin, channel 2 is the output voltage, channel 4 is the external load 750mA(the internal current of the product is about 200mA)