Other Parts Discussed in Thread: SN75LVDS83
We need to allow for inputs to be applied without VCC applied.
LVDS83A and B both have ESD clamps from input to VCC, this will allow backfeed into the VCC when unpowered and an input applied.
LVDS83 does not show the input clamps, and its ABS MAX spec on the inputs is 5.5V, the other two state VCC+0.5V.
Is it acceptable to have an input applied to the LVDS83 without its VCC applied?