Part Number: SN65LVDT32B
Tool/software:
Hi team - can you help with the below? Thanks!
Need some clarification please,
The esd rating table for SN65LVDT32BD is less clear than it could be:
Because here A is the noninverting receiver input, and B is the inverting receiver input. To say nothing of the gate pins, output pins, or VCC…
So are the A pins the only ones at 15kV rating? A and B only? Or are all pins on the device rated to 15kV?
But the SN65LVDS33D table makes the difference in rating between groupings of pins much more apparent:
Or am I reading that wrong?
So my question for both of them I guess is “what is the lowest ESD HBM rating any pin on the devices have?”