Part Number: TLK10232
Tool/software:
We have the TLK10232 sitting on an extender board to one of our switches - the TLK is connected to 2 XAUI interfaces on its LS side and to a processor with 10G-KR on its HS side.
During bring up of the extender board (and maybe also later on in the real application) we need to have the option to interconnect the 2 XAUI interfaces, i.e. bridging LS channel A IN to LS channel B OUT and LS channel B IN to LS channel A OUT respectively. Acc. to our interpretation of the data sheet this should be possible using the internal switch function of the TLK10232. The idea is, that this XAUI bridge on the LS side is possible regardless of the state of the KR interfaces on the HS side. The switch should be controlled by MDIO register access (i.e. not Pin controlled).
Could you please advise,
* if the intended functionality is supported by the TLK10232 device
* which register values should be used to configure this
* which limitations or special conditions/dependencies would have to be considered (if any).
Thank you very much in advance for feedback & support!
BR
Joerg