Part Number: DP83561-SP
Tool/software:
Hello, can you support the question below please:
I was reading about that part’s two-supply mode, and the datasheet has the following recommendation in section 9 on page 90:
“In the Two-Supply Configuration, no power rail is connected to VDDA1P8_x pins (pin 13, 48). When unused, pin 13 and 48 should be left floating with no components attached to them.”
In the Pin description section,
Pin 13 is TD_P_D and Pin 48 is TX_EN/TX_CTRL.
The VDDA1P8 pins are 16 and 64.
Just wanted to confirm, is this a typo or am I misinterpreting the documentation?
Thanks!
Owen