This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS1204: Pull-Down 499 Ohm resistors for AC-coupled operetion

Part Number: TMDS1204

Tool/software:

Hello,

Could you please clarify what are the goals of the MOSFET here:

  • Hi Nikita,

    The MOSFET allows you to control whether the 499Ohm terminations are enable or disabled. This is useful when you want to support the higher HDMI2.1 data rates.

    At lower HDMI1.4 and HDMI2.0 data rates, the 499Ohm terminations should be enabled to keep the common mode voltage in compliance with the HDMI spec. The issue is that at higher data rates, the 499Ohm terminations will pose a signal integrity concern as higher speed signals are more sensitive to terminations. If you're operating at HDMI2.1 speeds, you can disable the 499Ohm pulldowns using this MOSFET to improve the signal quality.

    Best,

    Shane

  • Ooo, I thought "System 3.3V" is a power rail, now it's clear, thank you!