This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812S-Q1: question about INH pin and resistor bootstrap

Part Number: DP83TC812S-Q1

Tool/software:

Helo,

I need information about:

1)INH is open drain but is not clear if this pin can accept a voltage about 12V

2)Pin boot strap (for example RX_DV and RX_ER these pins define PHY address) put RH resistor 4.5kohms tollerance 10%, if possible use 4.7kohms with 1%? because is difficutl to find this resistor value(hereunder a image)

Thank you in advanced.