Part Number: TUSB321
Other Parts Discussed in Thread: AM62A3-Q1, TUSB319-Q1
Tool/software:
Hello Team ,
In our application we need to Negotiate for the with laptop for Current Advertisement (5V@3A) using the Standalone CC Controller in UFP(Sink) Configuration.
Power is required to update the Firmware in our device connected to Laptop(Host) with our device.
Data Exchange between Laptop(Host) and our device will occur over USB TO ETHERNET BRIDGE IC (LAN7801).
(LAPTOP <---> USB TO ETHERNET BRIDGE <---> AM62A3-Q1 SOC)
So this is the use case ,For reference do refer the below block diagram.

Kindly purpose appropriate solution for our requirement !
Also the Part should be AEC qualified for Automotive application.
Regards,
Tirthal Patel