Part Number: DP83TG720S-Q1
Other Parts Discussed in Thread: DP83867E
Tool/software:
Hi Community,
I have a short question regarding my design for a SPE interface where I'm using the DP83TG720S-Q1.
The signal path is the following:
NVIDIA Jetson <--> Realtek Chip (PCI)
Realtek Chip <--> DP83867E (4 Lane Ethernet)
DP83867E <--> DP83TG720S-Q1 (RGMII)
DP83TG720S-Q1 <--> Connector (Single Pair Ethernet)
My design works and I get good data rate performance when testing the SPE.
The only thing where I'm still a bit uncertain about is, when I unplug the SPE cable the OS on the Jetson says that a connection is available, even if it is disconnected. When I boot the Jetson without an SPE cable attached, the OS shows that there is no connection, and when I plug in the cable the connection appears as it suppose to be.
The question I'm asking me is if this behavior can be fixed somehow, or if it is caused by all the components in the signal chain. I have to use this architecture to interface SPE, there is no other way to realize this in our system.
Does someone have experience with this?
Thanks a lot.
Regards Yannik