Part Number: DP83822I
Tool/software:
The DP83822I datasheet says that the 49.9 ohm resistors and capacitors must be placed close to the device. I've seen other PHYTER datasheets mention the same thing, so I'm 99% sure this is correct. However, when I look at the layout on the DP83822 EVM board, those 49.9 ohm resistors are placed right next to the magnetics. Is the EVM layout correct or the recommendation in the datasheet? I believe the datasheet is correct, please confirm.
The DP83822I datasheet also has 1uF and 0.1uF caps on the AVD supply that feed the 49.9 ohm resistors. The EVM doesn't have these caps. The power supply recommendation (section 10 in the datasheet) already calls out for 1uF and 0.1uF caps (in addition to others). It also recommends those caps be as close to the DP83822 as possible. Since AVD is pin 14, and the TP+/TP-/RD+/RD- pins are right next door, I don't see how the caps recommended in the datasheet (section 9.2.1) will make any difference. Is the EVM layout correct or the recommendation in the datasheet? In this case, I think the EVM is correct. Please confirm.
Thanks, Dean