Tool/software:
Dear Team,
We are using DP83822I Ethernet Phy IC in our controller for Ethernet application. We are using 1.8V supply for VddIO (21pin) & AVdd (14Pin). This Application, we want use LED-0 (17pin) & LED-1/GPIO1 (24Pin) power supply with 3.3V.
So please suggest this 3.3V can be connect these LED pins, If VDDIO & AVDD is connected to 1.8V Power supply. Due to LED drop is 1.9V max, so we want to connect this LED supply to 3.3V & Ground is same of 3.3V & 1.8V Power Supply.
Best Regards
Shiva Kumar T N
Sr. Engineer R&D.
MEDHA SERVO DRIVES PVT LTD.
Mail ID: shivakumart@medha.com