Part Number: LMH0070
Tool/software:
Hello,
In LMH0070SQE/NOPB SDI serializer IC, we have LVDS Differential Input pins which are TX[4:0]+, TX[4:0]- and TXCLK+, TXCLK-.
What is the input current rating of this pins?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH0070
Tool/software:
Hello,
In LMH0070SQE/NOPB SDI serializer IC, we have LVDS Differential Input pins which are TX[4:0]+, TX[4:0]- and TXCLK+, TXCLK-.
What is the input current rating of this pins?
Hi Shiva,
There is no validated input current rating for the pins. I can provide a general recommendation based on the fact that the TX pins are terminated by 100 ohms to GND and LVDS current is generally held constant at around 3.5 mA. The device is validated to standard LVDS so the pins are able to accept 3.5 mA.
Please let me know more about the application.
Best Regards,
Nick