Part Number: DS90UB949A-Q1
Tool/software:
Hello,
I'm planning to map the pins of the DS90UB949A-Q1 with the SoC signals and wanted some clarifications:
1️⃣ The DS90UB949A-Q1 has two I2C interfaces:
- DDC I2C
- Standard I2C
What are their specific use cases, and do both need to be connected?
2️⃣ SPI Pins & High-Speed Bidirectional Pins
- Can I leave these pins unconnected if not required, or are they essential for specific functionalities?
Additionally, if you have a hardware application note or design guide, that would be really helpful.
Regards,
Abhishek