This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK100 Default PD/PU States

I'm referencing the TLK100 datasheet (SLLS931B–AUGUST 2009–REVISED DECEMBER 2009) and my question involves the PHYAD[0:4] lines.  Page 6/88, Table 2.2 shows MII_COL/PHYAD0 being internally pulled UP by default while all the other PHYAD[1:4] pins are pulled DOWN.  Then, on page 8/88, Table 2.7 lists PHYAD[4:0], specifically including PHYAD0(MII_COL), as having all internal pull DOWN resistors.  Then, on page 15/88, it shows the default setting for PHY address as being 0x0h with all internal pull DOWNs; however, the figure below (Figure 3-1) shows PHYAD0 being internally pulled UP by default (with a conflicting note above the figure, might I add.).

 

I simulated the IBIS model for the TLK100 in HyperLynx and verified that PHYAD0 is internally pulled UP and PHYAD[1:4] are internally pulled DOWN.  Given the several inconsistencies, I'm sure you can understand my confusion/hesitation, but I am designing under the following assumption:  PHYAD0 is internally pulled up by default and PHYAD[1:4] are pulled down by default.  Is this a correct assumption?

 

Thanks in advance for your time and help!!