Tool/software:
Hi,
Our customer is considering using this IC for the following two purposes. Can we use it?
Application 1: MIPI-DSI BUS SWITCH
Two different LCDs are connected to the output destination of the SoC MIPI-DSI (CLK 1Lane + Data 4Lane), so we would like to switch between them.
→ P.19 Figure 9-8. Mipi DPHY based DSI switching. Would this be a problem if we use the configuration?
Application 2: RGMII BUS SWITCH
Two different Ethernet PHYs are connected to the output destination of the SoC RGMII (12bit in the table below), so we would like to switch between them.
→ IO voltage 1.8V, clock frequency 125MHz.

→ Can we switch by using all 12bits, SCL, SDA, D0± to D3±, HPD, CEC?
(SCL, SDA, HPD, CEC can also be used as Mux for high-speed signals.)
Best regards,
Hiroshi