Tool/software:
Hi,
I am looking for ethernet switch for our automotive application. I couldn't find the one but came across TS3USB221A-Q1. As this is for USB, can we use for ethernet and CAN protocol also?
Let me know if any appropriate solution is available.
Below is our requirement:
- Signal switching (ethernet 100-base, CANK/L line protocols ,etc.)
- Coil ratings (wide range from 3.3-12V with latching option is preferred to reduce consumption)
- Contact ( Input voltage: 0-36V operation, Current: 1A)
- Signal Frequency: >100MHz
- High frequency switch is not intended as there won't be a run time switching.
Thanks,
Nikunj