This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: Unused VBUS

Part Number: TUSB1210

Tool/software:

Good day,

Can the TUSB1210 device be used in Host mode with the VBUS pin not connected?

We will not be using the VBUS detect or CPEN. 

Should I leave the VBUS pin not connected, GND or just connect it to 5V and add a decoupling capacitor?

If I want to use it in Device mode, can I still have this connected to 5V and a decoupling capacitor?