Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4551-Q1: TCAN4551-Q1

Part Number: TCAN4551-Q1

Tool/software:

Hello Team,

I'm working on TCAN 4551 and implemented FIFO watermark feature. excepted watermark interrupt are received.

I have configured watermark level to 60, After receiving 60 messages, getting interrupt. Here i need timestamp of each received message.

Please guide me.

Thanks,

Amit 

  • Hello Amit,

    The TCAN4551-Q1 uses the CAN FD Controller IP called MCAN developed by Bosch.  I would refer you to the M_CAN User's Manual (Link) for additional information on how to configure and use the MCAN features including timestamps for messages.  The only thing to note is that the TCAN4551-Q1 has added a register offset of 0x1000 to each MCAN register address.  Therefore as an example, the Control register is listed as 0x18 in the M_CAN User's Manual, but is actually 0x1018 in the TCAN4551-Q1.  Otherwise, all of the other information in the M_CAN User's Manual is applicable to the TCAN4551-Q1.

    There is an “Internal” timestamp counter inside the M_CAN controller core that counts in multiples of CAN bit times. This is controlled in register 0x1020 (note this is an M_CAN register because of the 0x1000 offset). The Timestamp Counter Prescaler TCP[3:0] can be configured to count in multiples of 1 to 16 bit times as set with this register. The current Counter value can be read from register 0x1024 and at any time can be cleared or re-started by writing to 0x1024 if the “internal” counter has been configured for use. I will also note that I believe the device will use the Nominal Bit Times to count and does not count the FD bits which would overrun the counters too frequently.

    The M_CAN controller allows for an alternative “External” timestamp counter to be used instead of the internal CAN bit time counter and it simply takes a 16 bit value from this external counter, but it doesn’t specify how this external counter should be implemented. The TCAN451-Q1 uses a standard divider off of the Host Clock frequency (crystal/clkin) that allows for a divided down clock value to be used as the time stamp. If you select a TSCC.TSS[1:0] value of “10” (register 0x1020) then this “external” timestamp counter will be used. And by “external” it simply means that it is external to the M_CAN Controller Core. But since this is a TCAN4551 specific feature, its prescaler is setup in register 0x0804. Notice the address offset indicates this is not an M_CAN core register. By default this register has a value of 0x02, which will yield a clock divider of 16. Writing the pescaler value to this register will clear and re-start the Counter. When this counter is configured for use, the counter’s current value can be read in register 0x1024 which is the same register as the Internal counter since there is only one counter that can be used at a time.

    I will also note that you should add into the configuration routine a timestamp counter reset for which ever counter you chose to use so that once you start communicating on the CAN bus, you have a deterministic starting point for the counter values. Every time the counter wraps around, it will set an interrupt bit so that the MCU can keep track of how many times the counter has re-started. If this is important to you, I would suggest you have some form of secondary counter in the MCU to keep track of these wrap around interrupts which could be internally appended to the timestamp value captured from a message if the message is stored in some form of log.

    Regards,

    Jonathan

  • Hello Jonathan,

    I have configured the system as you mentioned in your previous message, and I am now receiving the timestamp count. As you mentioned, the timestamp counter gets reset (overflow), and I have configured the Timestamp Wraparound (TSWE) interrupt accordingly.

    I’m using a watermark interrupt with a threshold of 56, and I receive the interrupt after every 56 packets. Once the interrupt is triggered, I read all 56 packets from the FIFO. My question is: how can I track or determine the amount of time of TSWE interrupt occurred between two messages while reading the FIFO?

    Thanks & regards,

    Amit Sutrave

  • Hello Amit,

    The message timestamps will continue to be captured and stored with the message buffer elements in the FIFO.  When the counter wraps around, the new messages may have a counter value that is less than older messages already stored in the FIFO.  So, the overall difference in time between the reception of these messages will be the cumulative difference of the timestamps that would need to be calculated.

    Regards,

    Jonathan