Part Number: DP83826I
Tool/software:
I'm experiencing a hot-plug issue with the DP83826I PHY on Phytec STM32MP1 SoM with custom carrier board:
- When the system is powered on and I connect an ethernet cable:
- Orange LED stays solid ON (indicates 100Mbps connection)
- Green LED blinks (indicates activity/link)
- However, the interface cannot acquire an IP address
- If I reboot the system with the ethernet cable connected, it works perfectly and gets an IP
Is there a recommended register configuration (or any idea) to properly handle hot-plug scenarios? Also, is this LED behavior correct for a situation where IP acquisition fails?
Thank you for your assistance.
Regards