Part Number: THVD1410
Tool/software:
Dear Specialists,
My customer is considering RS485 transceiver and has questions.
I would be grateful if you could advise.
ーーー
(1) The THVD1410 has the Extended Common Mode notation, and the datasheet states that it has low jitter even outside the general RS-485 specifications.
Is it correct to assume that devices with the Extended Common Mode notation are suitable for long-distance transmission?
(2) I was considering SN65HVD2x as a replacement for the MAX22500E, is a fairly old device.
I would like to consider a newer product if possible.
Also, the built-in equalizer is effective at speeds of 1Mbps or more, and 1Mbps is only effective at long distances, so I am looking for a substitute product.
(3) Could you please provide the other device for high-speed long-distance transmission?
---
I appreciate your great help in advance.
Best regards,
Shinichi