Part Number: DP83822IF
Tool/software:
Dear Manager,
I'm using the PHY, DP83822IFRHBR.
I have the following questions while using it.
Please let me know how can I solve it.
- Desired setting
* 1. MLED rout to LED_0 : set bit[1:0] to 11 @0x0025
* 2. MLED configuration to TX activity : set bit[6:3] to 001 0 @ 0x0025
* 3. LED_0 blink rate to 20ms : set bit[10:9] to 00 @ 0x0018
- Good operation
* above 1, 2 setting
- Bad operation
* above 3.
* Even if I change the blink rate via bit[10:9] @ 0x0018 register, LED_0 always behaves the same.
- ex: when TX at every 500ms, LED_0 remains low for 350ms and then goes high for 150ms.
* The initial value of 0x0018 is 0x4000, and it was confirmed that it becomes 0x0000 after bing set to 20ms (0x0000)
- Question
1. How can I change the LED_0 blink rate?
Regards,
DaeJin