Part Number: MAX3232
Tool/software:
Hi all,
I am working on a design involving an RS232 connection between a stepper driver and a CPU board.
Now the tricky part is that the driver board needs to be hot swap-able. The stepper driver is built in a separate enclosure with a stepper motor.
The connection between the 2x boards is done via a 4 way connector: +24V, GND, TX (RS232 side), RX (RS232 side)
The 24V supply a 3.3V step down regulator for the electronic and the stepper motor. The TTL side of the MAX3232IPWR doesn't get disconnected.
This seems to damage the MAX3232 chip.
Would this be due to the RS232 signal or power being apply not quite on the same time?
How would one protect / prevent damage to the MAX3232 ?
Thank you for any help.
Laurent