Part Number: DS16F95
Tool/software:
Hello,
Considering using the DS16F95 in a receiver only configuration with low input data rates -- but the ICC Max value listed in the datasheet implies >100mW even in this configuration... Is this accurate / correct interpretation?

For further reference to the application -- toggle rate would be very low (once every several milliseconds ... I.E. < 1kHz data rate)
Should we be expecting up to 28mA (140mW) even in this very low toggle rate configuration?
If yes... out of curiosity... what is driving such high currents? The large common mode range biasing the inputs (we expect to be in a very narrow common mode range)? Or just internal biasing?