This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: TUSB9261+Windows11 is not being recognized

Part Number: TUSB9261

Tool/software:

Dear all

Hi!

I'm useing TUSB9261 on my PCB.

Now, I am having an issue on a specific PC not being recognized.

PC is Windows11, CPU:i9-14900KF and Chipset:Z790-S01.

Don't being recognized.

Do you have any information about TUSB9261 not being recognized?

Sincerely.

Kentaro Iba

  • Hi Kentaro,

    Does this device recognize on other PC's? Which firmware are you using? Are you getting an indication of it not being recognized like a yellow bang, or is the TUSB9261 board not even enumerating?

    Thanks,

    Ryan

  • Dear Ryan

    Thnak you for your response.

    Another Windows11 PC is  recognized TUSB9261, but Windows11, CPU:i9-14900KF and Chipset:Z790-S01 's PC is not recognized.

    I'll look into the following.

    > now firmaware version

    > ecognized like a yellow bang, or is the TUSB9261 board not even enumerating

    if dou you have new firmware, Can you provide it?

    Sincerely 

    Kentaro Iba

  • Hi Kentaro,

    We don't have any new firmware, I was wondering if you are using one of the firmwares we provide on TI.com, or if you developed your own firmware.

    Would it be possible to gather more information about this working Windows 11 PC, such as the CPU or chipset? Any other differences would be good too.

    Thanks,

    Ryan

  • Dear Ryan


    I'm using  firmware is provide on TI.com.

    > Would it be possible to gather more information about this working Windows 11 PC, such as the CPU or chipset?

    Anoter all PC is OK, CPU:i9-14900KF and Chipset:Z790-S01 's PC is not only recognized.

    > Are you getting an indication of it not being recognized like a yellow bang,

    USB TYPE C PC's connector:recognized , but not access SSD on TUSB9261

    USB TYPE A PC's connector:not recognized

  • Hi Kentaro,

    When it is recognized via the type-C, does it appear in device manager? What is it recognized as, I.E Disk Drive, other device. What is the name, VID and PID?

    Can you send over the schematic for this design for us to review as well?

    Thanks,

    Ryan

  • Dear Ryan

    Sorry for the late reply.

    I haven't heard back from the customer so please wait.

    Sincerely

    Kentaro Iba

  • Hi Kentaro,

    No worries, just let me know when you have anything.

    Thanks,

    Ryan

  • Dear Ryan

    Since I haven't received any feedback from my customer, I will close this ticket for now.

    Thank you so much!

    sincerely