This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043A-Q1: TCAN1043A-Q1

Part Number: TCAN1043A-Q1

Tool/software:

Hello, I want use TCAN1043A-Q1 as a bus activity monitor for some bench work I am doing. My plan is to use the RXD signal along with an LED driver to display bus activity.
I want to confirm that I am connecting the IC up correctly as a stand-alone bus monitor.

pin 1 TXD Connect to 5V since I won't be transmitting
pin 2 GND
pin 3 VCC to 5V power from regulator
pin 4 RXD to the LED driver to display bus activity
pin 5 VIO to 5V
pin 6 Enable to 5V
pin 7 INH no connection
pn 8 nFault no connection
pin 9 Wake no connection
pin 10 Vsup to 12V same as input to 5V regulator
pin 11 no connection
pin 12 CAN L
pin 13 CAN H
pin 14 nSTB connect to 5V

My next question is, does this Chip work with CAN FD and J1939 as well as standard CAN?

Thanks!