Part Number: DS90UH981-Q1
Tool/software:
When do we need to operate the PORT_SEL register? If using the indirect registers (0x40~0x42) in 981 to access the DPHY_SKIP_TIMING register in page 4, how do I set the PORT_SL register?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH981-Q1
Tool/software:
When do we need to operate the PORT_SEL register? If using the indirect registers (0x40~0x42) in 981 to access the DPHY_SKIP_TIMING register in page 4, how do I set the PORT_SL register?
Hi Zhouyi,
The PORT_SEL register should be utilized when operating the UH981 serializer in a Y-split configuration (when port 0 is connected to one deserializer and port 1 is connected to a separate second deserializer). In these Y-split configurations, certain port-specific registers have two copies of the register - one for each FPD-Link port. Toggling this PORT_SEL bit is what allows you to read/write to the desired copy of these port-specific registers.
The PORT_SEL register is not required when accessing the DPHY_SKIP_TIMING registers as there are already two devoted indirect pages for each separate DSI input port.
Let me know if you have any additional questions.
Best,
Nikolas