Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9539-Q1: Is the IO level following VCC?

Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCAL6416, TCA6416A

Tool/software:

Is the IO level following VCC, or is it allowed as long as the voltage is less than VCC? If VCC is 3.3V, is the IO level allowed for both 1.8V and 3.3V, or can it only be 3.3V