Part Number: THVD2410
Tool/software:
Hello guys,
One of my customers is considering using THVD2410 for their next products.
But they are considering using ADI, LTC2862AIDD-2 too because LTC device has higher ESD HBM ratings than THVD.
THVD2410 HBM : 16kV (Bus terminals)
LTC2862AIDD-2 HBM: 40kV (Human Body Model, A or B to GND, VCC, B or A, 1μF Between VCC and GND)
I think LTC test condition is different from THVD because 1uF capacitor is attached between VCC and GND in case of LTC device.
Our current question is the follow.
Q.
Can THVD2410 HBM performance achieve 40kV if the test condition is same as LTC2862AIDD-2 one?
Your reply would be much appreciated.
Best regards,
Kazuya.