Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Tool/software:
Dear Team,
We are using TCAN4550 with iMX8DXL processor lpspi. We have configured two CANFD to be connected two different SPI lines with two different TCAN chip. Now the issue is if we do the TX with single CAN we are getting throughput of around 5.5k msg/sec but when we do TX with both CAN in same arbitration and bitrate combination the throughput in each can will be reduced to half, like each CAN node transmits of around 2.7k messages per second which is not expected. So is there any way that you can help us to fix this issue.
Regards,
Ankita