Tool/software:
Hello,
My customer is using the TUSB217A with VCC = 5V (VBUS, same supply as the USB device they're testing). Do you expect any changes to the device behavior/performance if they move to a 3.3V supply?
My thoughts based on the datasheet:
The TUSB217A supports 3.3V (2.3-6.5V), but it does appear that some specifications are dependent on VCC. For ex., VIL and VIH(min) for Input RX_SEN (pg. 7 of DS).
I see in Table 9-1 that the 37.5kohm resistor is required for a 5V supply to divide the voltage down so the RX_SEN pin voltage does not exceed 5V. It appears this resistor is not needed for 3.3V supply.
They may want to review their BOOST setting to confirm it’s optimized after switching to 3.3V VCC.
Do you agree? Anything else we should highlight?
Best Regards,
Brian