Part Number: TPS53819A
Other Parts Discussed in Thread: LM5171, TPS40077, TPS40057
Tool/software:
Hi,
We need the buck DC/DC, and input is 24V, output is 12V/40A, please advise if the TPS53819A is available or not? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
https://www.ti.com/product/TPS53819A
It is listed as active and orderable. You'll need to log in to view inventory
My apologies for misunderstanding you question.
No, the TPS53819A does not support a 12V output, it has a maximum rated output voltage of 5.5V. This is due to the maximum voltage rating on the VO pin of 6V, and the internal compensation ramp's linear operating range.
For a 20V - 26V input, 12V Output @ 40A, the only non-isolated solution I see using the WeBench Power Designer tool is the LM5171
https://webench.ti.com/power-designer/switching-regulator/select
https://www.ti.com/product/LM5171
It may also be possible to design a TPS40057 or TPS40077 controller to operate at 40A output current, but the integrated drivers were not indented to drive MOSFETs for a 40A power stage.