Part Number: TCAN1043HG-Q1
Tool/software:
Hi Expert,
Can you provide TCAN1043HG-Q1 external schematic devices parameter calculations tools?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1043HG-Q1
Tool/software:
Hi Expert,
Can you provide TCAN1043HG-Q1 external schematic devices parameter calculations tools?
Hi Sean,
Pls refer to our EVM schematic:

Question: The application is 48V BMS. How to calculate C2, C6, C7, L1 value?
Eric has given preliminary instructions: (+) TCAN1043HG-Q1: Components Evaluation in 5Mbps - Interface forum - Interface - TI E2E support forums. But that's not enough, customer wants a clear calculation formula or theoretical Explanation. Hope to get your support, thank in advance.
Hi Beida,
Eric's reply is exactly we will recommend for all CAN applications using our chips, we do not design system or require a single component, thus we can only recommend the typical value, it is customer's willing to choose a specific value to meet their system's requirements.
For the split capacitor C6, refer to the 4.5.2 in this app note.
https://www.ti.com/lit/an/slla270/slla270.pdf
For the bus filters C2 and C7, it's simply used to filter out high frequency noise, different capacitors can handle different frequency ranges but typically low value caps filter high frequency and higher value caps filter lower frequency. Adding capacitive load will increase the rise/fall time so they need to pick a value that can work well in their system.

For the choke L1, refer to this app note.
https://www.ti.com/lit/an/slla271/slla271.pdf
51uH - 100uH range is high enough to filter out common mode noise while being low enough to not heavily impact the CAN data itself or contribute negatively to transient behaviors through inductive kickback. This range is pretty standard throughout the industry. Our EMC test reports also use 100 uH.
Regards,
Sean