Part Number: TCA5013
Tool/software:
Hello,
We have several designs using the NXP TDA8026. This part is going obsolete.
We would like to replace it with the TCA5013. I have the following questions :
1) From the CPU, we have only one CLK and one I/O to drive all the four SAMs. Is it possible to connect IOMC1 to IOMC2 and CLK1 to CLK2 ? Of course, when we will adress card slot, we will disable the SAM IOSx pin and when we will adress SAMs, we will disable IOUC pin (using register 0x01 field name IO_EN_UC, and registers 0x11, 0x21, 0x31 field name IO_EN_SAMx)
2) Is ther any way to get/purchase TCA5013EVM board ?
Regards,