Part Number: SN75179B
Other Parts Discussed in Thread: THVD1426, THVD1520
Tool/software:
We are using the SN75179B for RS485 and we think the termination resistors are not correctly setup. During testing we see the transmit reflected on the receive pin. We believe this fs from the R38 termination resistor. We have the circuit setup for 122 ohms. Does this IC get setup different from typical RS485 transceiver with a DE and RE enables? I was looking through the datasheets, do we need to be doing the termination resistors separately on each drive (A,B) and receive (Z,Y) to power and ground for bias instead? Any help would be appreciated. Below is our current setup.