Part Number: TUSB320
Other Parts Discussed in Thread: MSPM0G3507, , BQ25622
Tool/software:
Hello,
Before starting, I'd like to mention that I'm new to embedded systems so I might lack some critical, trivial background information in this field. I would appreciate your patience.
I'm trying to connect TUSB320 to MSPM0G3507 and BQ25622 to develop a prototype for a battery pack eventually.
(So only power transfer is expected, and no data exchange will happen through the USB-C port.)
While designing a schematic for TUSB320, I found this example from the TUSB320 datasheet, but quite not sure about whether the 150uF bulk capacitor and the connected MOSFET are necessary to my design.
Since it's a prototype design for a student-level project, I'm not planning to make the battery pack compatible with legacy USB2 protocol - it's expected to follow just standard USB-C protocol (USB3.x I believe).
In this case, are the FET and the 150uF bulk capacitor (marked with yellow highlighter in the example schematic from the datasheet below) needed for the design? Or is it ok to connect VBUS to PMIC without the FET and the bulk capacitor to achieve a successful setup for DRP configuration?
Also, if the FET and the bulk capacitor are needed, could you let me know which type of FET should I choose? Should it be NMOS or PMOS? Are there any other parameters (operation voltage range, etc.) that I need to carefully pay attention to when choosing the FET?

I appreciate your help and time.
Thank you!