Part Number: THVD4411
Other Parts Discussed in Thread: THVD4421, THVD4431
Tool/software:
I am trying to build a 232/422/485 circuit using the THVD4411.
Before that, I have some questions, so I will leave them here.
1. Regarding RS232 settings (MODE1/0 = L/H)
a. Is the setting of "DIR" PIN Don't care, or should I set a specific state among H/L?
b. Is the setting of "TERM_TX/RX" Don't care, or should a specific state be set between H/L?
2. Regarding RS485 Full duplex setting (MODE1/0 = H/L)
a. Is the setting of "DIR" PIN Don't care, or should a specific state be set between H/L?
3. Inquiry regarding RS422
a. If RS485 full duplex setting and physical wiring are RS422, is RS422 communication possible?
That's all.
Waiting for your reply.