Part Number: TLIN1021A-Q1
Tool/software:
Hi,
1.When TXD=0V VLIN=18V, what is the duration of the short circuit current (max.200mA)? How much will the supply current increase? What is the duration?In addition, how does the chip state change after a short circuit?
Does the LIN chip continuously send the dominant level (although the bus is forced to 18V) to the tTXD_DTO release the bus? Or is there some other mechanism to shorten the time of this failure (max.200mA bus current inflow)? If so, what is the duration of the failure (200mA bus current inflow)?
2.For some LIN chips, if the CI 85V capacitor is directly coupled to the test, the chip will be damaged, so a 10Ω resistor in series is required to limit the current. If 85V direct capacitive coupling test is carried out on SN1021 chip, will it cause chip damage? In other words, is it necessary to have a 10Ω resistance in series on the LIN bus?
3.Regarding False Wake Up Lockout, is this mechanism automatically activated when the chip enters sleep-mode with the bus holding the dominant level?
4.As for the time to hold EN high to complete the wake up, is it tNOMINT? Or is it tmode_change? Or tNOMINT+tmode_change?


Best wishes