Part Number: ONET1151L
Other Parts Discussed in Thread: ONET1101L
Tool/software:
Hi,
For ONET1151P and ONET1151L the datasheet states SDA as digital-input. Can you confirm if SDA here is bi-directional?
For ONET1151L, the following application report says that the ONET1151L MOD+/- pins are 500ohm differential back terminated for low-power designs and that an impedance matching circuit is critical.
https://www.ti.com/lit/an/slla335/slla335.pdf
The datasheet says MOD+/- are 25ohm single-ended back terminated (50 ohm differential back terminated). Is this the default setting? Setting ORADJ to 00 is the lowest-output termination which is the 25 ohm nominal but setting ORADJ to 11 results in the highest output resistance. Is this how to achieve the 500ohm differential back termination? The goal of all this is to determine if the impedance matching circuit is necessary. Ideally I would not want to add it so please comment if it is not needed or recommended when using the 25ohm single-ended back terminated setting.
Thank you!