Part Number: DP83822I
Other Parts Discussed in Thread: AM2432, , DRA821
Tool/software:
Dear Team,
My customer is evaluating the DP83822I with Processors, DRA821 and AM2432.
When the customer changed the RX_D3 setting of the DP83822I from MODE2 to MODE1 to enable the Auto Negotiation, Processor, DRA821 or A2432, can not access the DP83822I. Although, PHY Address is not changed.
When the RX_D3 has external pullup 10kΩ and pulldown 2.4kΩ for MODE2, Processor can access the DP83822I by PHY_ADD="00000".
But when the RX_D3 is open for MODE1, Processor can not access the DP83822I by PHY_ADD="00000".
Please review an attached below.
DP83822I RX_D3 PHY_AD4 issue.xlsx
Do you know what is causing this issue accessing the PHY address?
Best Regards,
Koshi Ninomiya