This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848Q-Q1: Trace Length Matching Requirement for RMII Interface

Part Number: DP83848Q-Q1

Tool/software:

Hello,

We would like to clarify which traces need to be length-matched in RMII mode.

In MII mode, both the TX_CLK and RX_CLK are used, and all data lines(TX[1:0],RX[1:0]) are length-matched with these clock signals. However, in RMII mode, the X1 input is used as the clock reference.

Our question is: do the lengths of the data lines(TX[1:0],RX[1:0] and other RMII traces) need to be matched to the length of the X1 input trace, from the clock source to the PHY and MAC?