Part Number: DP83TC812EVM-MC
Other Parts Discussed in Thread: DP83TC812R-Q1,
Tool/software:
Hello,
Can I communicate with a different chip for the DP83TC812 family?
I have 3 devices;
One of them has DP83TC812R-Q1 eth
One of them is DP83TC812EVM-MC card
One of them has BCM89836 eth
Normally I tried to enter sleep mode on DP83TC812R (slave) via BCM89836 (master). It didn't work. Then I decided to test with DP83TC812EVM and BCM89836. I used BCM89836 as slave and used DP83TC812EVM-MC as master.
I sent the value 0x0002 to EVM via MDIO in register 0x018C. If EVM and DP83TC812 devices are connected to each other, both devices will enter sleep mode. But if you connect DP83TC812EVM to BCM89836, the devices do not go to sleep mode. In both tests, EVM is master. (I assumed that it would be easier test in the EVM master case.)
My main goal is to send a sleep command from BCM89836 using TC-10 and put DP83TC812 to sleep.
How can I do this?
Best Regards,
Faruk