Part Number: MAX3232E
Tool/software:
MAX3232EIPWRQ1 IS USED FOR DIAC APPLICATION ON A COMPLEX COMMUNICATION BOARD , HAS A UNIQUE ISSUE WHERE ONLY THIS IC OUT OF 30 IC ON THE BOARD FAILS OR OUTPUT IS JUNK CHARACTER AFTER DIPPING IN DIP COATING NANO COATING SOULTION PROMOSOLV UT10 2% USED FOR PROTECTION SIMILAR TO CONFORMAL COATING .
PRODUCT WORKS FINE BEFOR COATING BUT AFTER COATING IT FAILS
ON REPLACING THE IC WITH ANOTHER NEW IC WITHOUT COATING , THE BOARD WORKS FINE (SWAP TEST)
INPUT/ OUTPUT FOR THE DIAC IS CONFIGURED THRU USB
ANY SUCH REPORTING OR KNOWLEDGE WHY THIS HAPPENS.