Part Number: MAX3232
Tool/software:
CAN WE USE USB 3 PORT FOR DIAC PURPOSE , WHAT ARE THE PRECAUSION TO BE FOLLOWED DURING SUCH CIRCUIT CONNECTIONS FOR LOADING OR PROGRAMING
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3232
Tool/software:
CAN WE USE USB 3 PORT FOR DIAC PURPOSE , WHAT ARE THE PRECAUSION TO BE FOLLOWED DURING SUCH CIRCUIT CONNECTIONS FOR LOADING OR PROGRAMING
Hi Deepak,
I don't know what you're specifically asking. The RS232 devices usually are used with UART as the software protocol but technically you could use it for something else as long as the signal is uni-directional and the datarate is supported by the device.
-Bobby
But i am more interested to understand the the failure % and also using the USB Typr A for input and output , as there is 16% failure when we use usb type A for input/output .
If you could put some knowledge on this .will be happy