Part Number: DS90UH947-Q1
Other Parts Discussed in Thread: DS90UH948-Q1
Tool/software:
Dear, TI
We are using the DS90UH947-Q1 & DS90UH948-Q1.
It consists of MAIN SET and MONITOR as shown in the figure below. Rosenberger HDS cable is used as the connection cable.
The problem occurs when the length of the Rosenberger cable is long.
It works normally with a 1m cable, but with a 5m cable, the screen don't output(black screen), the touch don't work, etc.
We need to use a 5m cable, so please check if there is an IC that can be used as an amplifier or pre-amp for FPD LINK III.
Or, please also check if there is a way to increase the internal signal strength of the DS90UH947-Q1.
Thank you, for your support.
Best regards,
GH Park