Part Number: SN75DP122A
Tool/software:
Hi,
I have a question about the HPD pin.
Currently, it is connected with CPU - SN75DP122A - HDMI connector structure.
DP is unused, PRIORITY pin and LP pin are set to High, and TMDS pin is connected to HDMI connector.
Looking at the datasheet, it seems that 100K Pull down is applied, but don't you usually put a Pull up resistor between SN75DP122A - HDMI connector?
I wonder which one is correct.