The device I received is marked as 'A5' but that is not listed as an option in the datasheet.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The device I received is marked as 'A5' but that is not listed as an option in the datasheet.

This is a known issue where parts out of a specific manufacturing site were marked with an incorrect device marking. Because the 'A5' is an incorrect marking for the device, 'A5' will not show up in the datasheet. Any device received with 'A5' has no functionality, quality, or reliability issues. The performance of the device was not affected.
An audit has been conducted to understand why this occurred and moving forward all devices affected have been corrected to a device marking listed in the datasheet. There is material circulating with 'A5' and this will most likely be the case for the next year or so until the material has made its way through the system. Devices with a manufacturing date code after 11/17/2024, should not show 'A5'.
Devices affected are listed below along with ALL suitable device markings:
Please reach out for any questions.