Part Number: SN65LVDS31-32EVM
Tool/software:
Hello, may I please have the updated mounting hole dimensions (6 holes) for the SN65LVDS31-32EVM? The dimensions provided in this thread seem to be out-of-date.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVDS31-32EVM
Tool/software:
Hello, may I please have the updated mounting hole dimensions (6 holes) for the SN65LVDS31-32EVM? The dimensions provided in this thread seem to be out-of-date.
Hi,
I am looking at the diameter of the mounting hole and it is still 0.16in.

Thanks
David
Hi David,
May I please have the following updated dimensions from the previous thread?
- Board length
- Board width
- Board Height
- Distance from edges to each hole center (2 measurements for each hole so 12 measurements in total unless they are the same distance from the edges)
- Hole Diameter: 0.16in.
Seems like board length and width have decreased since that thread.
Hi,
I am looking at the board width and length and they are still the same, 6.5 x 2.5.

Board thickness is 0.0622in.
Distance from edges to each hole center is 0.25in.
Thanks
David
Hi David,
Thank you for the information. For distance from edges to hole center, I'm measuring 0.30in., is it possible to confirm this dimension?
Hi,
You are correct, I am also seeing 0.3in in my measurement as shown below.

Thanks
David