This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD12S016PWREVM: TS3DV642A0RUAR, TCA9517ADGKR, TS3L501E

Part Number: TPD12S016PWREVM
Other Parts Discussed in Thread: TS3L501E

Tool/software:

What is the Maximum Junction Temperature(Tjmax) of the below mentioned parts and the copper wire bonds used in these parts are AEC qualified ?

TPD12S016PWR

TS3DV642A0RUAR

TCA9517ADGKR

TS3L501E

  • HI Anitha,

    The Tjmax of the components you listed are not released. All of them should be operated within operating free-air temperature -40 to 85C (Q1 version of them will be up to 125C).

    The components you listed are not AEC qualified. The Q-100 qualified parts will be have a Q1 at the end of their PN.

    For example, TCA9517ADGKR is not AEC qualified, and TCA9517DGKRQ1 is AEC qualified.

    BR,

    Ke Wang