Tool/software:
Thanks for your excellent APP note on how to configure the DP83826 for EtherCAT applications.
We're currently connecting two of these PHYs to an Infineon XMC4800 chip.
In our design we followed all the strapping guidelines for Enhanced Mode in figure 3-1.
In this case, the PHY1_LED1 signal is strapped to GND. This causes the LED polarity auto-detect circuit to configure this signal as active HIGH.
This signal is meant to be tied into the EtherCAT controller on the PHYx_LINKn signal which is active LOW.
In section 2 of your EtherCAT Specification Requirements and Recommendations, there are two requirements related to this:


The first requirement says that the signal should be active LOW. The second requirement requires that the PHY be configured without the MII management interface. If I follow the suggested strapping in figure 3-1, the LINK signal in the first requirement is driven active HIGH.
We had to re-spin the board to add an inverter for this LINKn signal.
I'd recommend adding an inverter to your Enhanced Mode Example (or at least a note pointing out the polarity) so that other designers don't encounter the same issue.
Thanks!
Tim Kutscha
Simplexity Product Development