Part Number: TCAN1044-Q1
Other Parts Discussed in Thread: ESD2CAN24-Q1
Tool/software:
1. One of our customer is using CAN IC in 2Wheeler speedometer.Speedometer get power from battery. Two type of batteries customer is using. Only issue in type B battery
2. There are two types of batteries :
a) Type A Battery: One is high side cut off i.e Bat +ve lines get cut when fault happens , while Bat- remains there
b) Type B Battery: THis is low side cut off i.e Bat +ve remains when fault happens , while Bat- cut off is there
C) speedometer has 4 pin connector: bat+ , bat- , canh, canl
Speedometer get power from bat+ and bat-
3. Earlire in filed customer used to get CAN got damaged issue
4. Then they connected ESD diodes at CANH & CANL. Now ESD started getting damaged in field
5. THen they increased ESD diode power, so now track getting burst in field
6. ESD are connected near to output board.
7. Plz advise what could be issue? Plz suggest suitable solution